Poskusite iskati po ključnih besedah, šifri izdelka ali številki naročila ali serijski številki, npr. „CM442“ ali „tehnične informacije“
Za začetek iskanja vnesite vsaj dva znaka.
  • Zgodovina

Drinking water analysis panel at Grand Belfort in France

Reliable, modular equipment for continuous monitoring of water quality

When it comes to guaranteeing the quality of drinking water, some analysis parameters are crucial and play a major role in monitoring the efficacy of the treatment process. It is therefore inevitable that these parameters are continuously monitored during the different stages in the production of drinking water. These include monitoring of chlorine, turbidity, dissolved oxygen and conductivity, according to the remineralization process performed on-site.

Water treatment plant in Belfort in France ©Endress+Hauser

The drinking water treatment plant Grand Belfort in France

Information on the installation and commissioning of Endress+Hauser physico-chemical analysis panels in the drinking water plant of Grand Belfort

Results

  • Tailor-made solution adapted to the regional needs

  • Time savings and increased productivity thanks to real-time monitoring of the relevant parameters

  • Reduced water loss despite bypass installation

  • Compliance with the water quality standards required by French legislation

The analysis panels meet all requirements of the waterworks in Belfort

We wanted equipment able to generate alarms, provide constant communication and, most importantly, warn us in the event of a problem with a parameter.

Laurent Godot, Manager
Grand Belfort drinking water station

The initial situation at Belfort

The drinking water plant in Grand Belfort supplies drinking water to more than 18,750 households in the west of France, which means that violation of legal requirements can not be tolerated. The Endress+Hauser analysis panels provide a tailored solution which fully meets the plant’s needs of reliable networked equipment, the ability to generate alarms and the possibility to monitor the production of drinking water directly.

Our Solution

Equipped with elven analysis panels, the drinking water production process at the Grand Belfort plant is monitored very closely by the suite of measurement sensors installed. The panels offer an unique solution to guarantee in real time, that the water treatment process is running correctly. They were all specifically created for each installation station. Sensors were installed to allow the key parametersto be monitored at each stage of the treatment process.