Poskusite iskati po ključnih besedah, šifri izdelka ali številki naročila ali serijski številki, npr. „CM442“ ali „tehnične informacije“
Za začetek iskanja vnesite vsaj dva znaka.
  • Zgodovina

Efficient sludge treatment and process control in real time

Reliable measurement of total solids for wastewater treatment plant Bändlegrund with Proline Teqwave MW 500

Due to increasing legal requirements, wastewater treatment plants are continuously required to review their processes and optimize them, if necessary. In this context, operators of the Bändlegrund wastewater treatment plant in Weil am Rhein, Germany saw potential for optimization in sludge management. The installation of the Proline Teqwave MW 500 in-line measuring device from Endress+Hauser made it possible to optimize multiple areas at the same time.

Picture of Bändlegrund wastewater treatment plant in Weil am Rhein, Germany ©Endress+Hauser

Bändlegrund wastewater treatment plant in Weil am Rhein, Germany, has existed since 1983 and currently has a capacity of 290,000 PE.

Picture of Proline Teqwave MW 500 measures the total solids in sewage sludge at Bändlegrund ©Endress+Hauser

Proline Teqwave MW 500 measures the total solids in sewage sludge in real time using microwave transmission.

The result

  • Increased operational safety thanks to process stabilization

  • Reduced energy and polymer consumption due to optimized sludge treatment

  • Process control in real time

  • Minimized manual effort and optimized pump runtime performance

  • Increased digester gas yield

Steffen Mehlhorn, 
Managing Director of the Wieseverband 
wastewater association

"For us, it was very important that we optimize process control in sludge management in light of the increasing legal requirements in operation. We achieved this thanks to Teqwave MW 500."

Steffen Mehlhorn, Managing Director
Wieseverband wastewater association

The customer requirement

One optimization approach was the removal of primary and secondary sludge from the hoppers of the primary clarifiers. This process was controlled by the runtime of the sludge removal pumps. Adjusting the runtime required the results of a manual sludge level measurement and experienced personnel. Another challenge is the solids-based polymer dosing when dewatering the slurries. The solid content was determined manually and the amount of polymer was added in proportion to volume.

Our solution

Teqwave MW 500 is an in-line measuring device that displays the total solids in sewage sludge in %TS in real time using microwave transmission. Thanks to direct measurement in the inlet to the thickener, the flow of sludge can be balanced and pump runtimes can be automated. During sludge dewatering, real-time solids measurement enables the amount of polymer to be dosed in the inlet of the chamber filter press optimally at all times, even in case of changes to the solids content.

  • Enostavni produkti

  • Lahka izbira, vgradnja in uporaba

Tehnična odličnost

Preprostost

  • Standardni produkti

  • Zanesljivi, robustni, nezahtevni za vzdrževanje

Tehnična odličnost

Preprostost

  • Vrhunski produkti

  • Visoko funkcionalni in praktični

Tehnična odličnost

Preprostost

  • Specialni produkti

  • Zasnovani za posebej zahtevne aplikacije

Tehnična odličnost

Preprostost

Spremenljivo

FLEX izbira Tehnična odličnost Preprostost
  • F
  • L
  • E
  • X

Segment Fundamental

Zadostite svojim osnovnim merilnim potrebam

Tehnična odličnost
Preprostost
  • F
  • L
  • E
  • X

Segment Lean

Obvladajte ključne procese na preprost način

Tehnična odličnost
Preprostost
  • F
  • L
  • E
  • X

Segment Extended

Optimirajte procese z inovativnimi tehnologijami

Tehnična odličnost
Preprostost
  • F
  • L
  • E
  • X

Segment Xpert

Imejte pod nadzorom najzahtevnejše aplikacije

Tehnična odličnost
Preprostost

Spremenljivo