Reliable technology for precise optical oxygen measurement
ArticleVeč industrij09.12.2025
Na kratko
Definition: Quenched fluorescence (QF) or fluorescence quenching is an optical principle that relies on the presence or absence of oxygen to affect the intensity and wavelength of a fluorescent material. This change in intensity and wavelength of the emitted light can be directly correlated to oxygen concentration in the process gas.
Benefits: Advantages include a fast and precise response to oxygen changes, the ability to measure oxygen down to very low (part-per-million) concentrations, high selectivity and immunity to interferences from gases such as CO₂ or H₂S, low maintenance with no consumable parts or reagents, and stability and safety provided by solid-state optical components for long service life.
Applications: QF technology is used across industries for oxygen monitoring in natural gas processing, energy transition, bioprocessing, environmental and water quality studies, and medical or Life Science research.
Technology: The spectrometer uses an LED to send visible light through a fiber optic cable to an oxygen-permeable coating containing a fluorescent dye. Oxygen alters the dye’s emitted light intensity and wavelength, which the analyzer measures. Using the Stern-Volmer equation, the system calculates oxygen concentration from these measurements.
Kazalo vsebineKazalo vsebine
What is quenched fluorescence (QF)?
Quenched fluorescence (QF) — also known as fluorescence quenching — is a fundamental photophysical process that plays a vital role in modern spectroscopy, measurement technology, and molecular analysis. It has become an essential tool for real-time oxygen measurement in natural gas processing, bioprocessing, environmental monitoring, and medical diagnostics. Its appeal lies in its precision, selectivity, and stability — achieved without the moving parts, chemical consumables, or cross-sensitivities common to older sensor designs.
This article explores the underlying physics of quenched fluorescence, its detection methods, practical implementations, and how it compares to other optical and electrochemical approaches used for gas measurement.
The fundamentals of fluorescence
When a molecule absorbs light energy, it transitions to a higher electronic energy state — a process known as excitation. As it returns to its ground state, the molecule releases some of that absorbed energy as visible or near-visible light. This re-emitted light is called fluorescence.
Fluorescence occurs only for molecules with specific electronic structures — often organic dyes or transition-metal complexes. The emitted light usually has a longer wavelength (lower energy) than the absorbed light due to internal energy loss during relaxation. The difference between the absorbed and emitted wavelengths is known as the Stokes shift, a concept central to fluorescence-based sensing.
Mechanisms of quenched fluorescence
Quenched fluorescence occurs when something causes a change in the fluorescent molecule emitting light after excitation. The “quencher” — typically another molecule — interacts with the excited state of the fluorophore, enabling it to lose energy non-radiatively (through collisions or energy transfer) instead of emitting a photon.
There are several mechanisms of quenching, including:
Dynamic (collisional) quenching: Energy is transferred to the quencher during molecular collisions in the excited state.
Static quenching: A non-fluorescent complex forms between the fluorophore and quencher before excitation.
Energy transfer and electron transfer: Energy or electrons are exchanged between species, reducing fluorescence yield.
In many industrial sensing applications, oxygen (O₂) serves as the quencher. Because oxygen efficiently deactivates the excited states of certain dyes, changes in fluorescence intensity or lifetime can be directly related to the oxygen concentration in the surrounding medium.
The Stern-Volmer relationship
The quantitative relationship between quenched fluorescence and quencher concentration is expressed by the Stern–Volmer equation:
I₀ / I = 1 + KSV[Q]
Or equivalently using fluorescence lifetime:
τ₀ / τ = 1 + KSV[Q]
Where:
I₀ and τ₀ are the fluorescence intensity and lifetime without quencher.
I and τ are the corresponding values in the presence of quencher.
KSV is the Stern–Volmer quenching constant.
[Q] is the quencher concentration.
The linearity of this relationship provides the basis for quantitative sensing. By monitoring the change in fluorescence intensity or lifetime, the concentration of the quencher — such as dissolved or gaseous oxygen — can be determined precisely.
Optical oxygen measurement and techniques
The basic measurement cycle
Optical oxygen sensors rely on the principle that oxygen molecules can “quench” the fluorescence of an excited dye. The measurement typically follows these steps:
Excitation: A light source, often a blue LED (≈470 nm), illuminates a fluorescent dye immobilized in an oxygen-permeable matrix.
Emission: In the absence of oxygen, the dye emits bright red or near-infrared fluorescence.
Quenching: When oxygen is present, it collides with the excited dye molecules and transfers energy non-radiatively, reducing the fluorescence intensity and causing a shift in wavelength.
Detection: The emitted light returns via an optical fiber to a photodetector, where phase shift is measured.
Computation: The system calculates oxygen concentration using calibration constants derived from the Stern–Volmer relationship.
Figure 2: Blue light excites the sensor tip to emit fluorescence; oxygen molecules quench this emission by absorbing energy, reducing light output.
This cycle allows real-time, non-consumptive oxygen measurement with remarkable sensitivity — from parts per million (ppm) levels up to percent concentrations.
Measurement techniques
There are two primary techniques used to quantify quenched fluorescence: intensity-based detection and lifetime or phase-shift detection.
Intensity-based detection: In early optical oxygen sensors, the decrease in fluorescence intensity relative to a reference was used to infer oxygen concentration. However, this method is somewhat sensitive to light-source variations, dye aging, and optical alignment.
Lifetime or phase-shift detection: Modern fluorescence-quenching sensors use phase-modulated light sources to measure the time delay (phase shift) between the excitation light and the emitted fluorescence. Because fluorescence lifetime is an intrinsic molecular property, this method is far less affected by environmental conditions or light intensity changes.
The fluorescence lifetime typically decreases from microseconds to nanoseconds as oxygen concentration rises. This phase-based approach enables fast response times, long-term stability, and high immunity to drift — key advantages in industrial applications.
The physics of quenching
Quenched fluorescence is fundamentally a process of energy transfer through collisions between excited fluorophores and quencher molecules. For oxygen quenching, this interaction is governed by diffusion kinetics and molecular orbital overlap.
The efficiency of quenching depends on factors such as:
Diffusion rate of oxygen through the sensor matrix
Temperature (affecting diffusion and collision frequency)
Viscosity and structure of the host material
Excited-state lifetime of the fluorophore
By tailoring the composition and porosity of the polymer film, engineers can control the diffusion rate of oxygen and optimize sensor response time and sensitivity.
Fluorescent sensor layer (dye matrix): A solid polymer or sol-gel film doped with an oxygen-sensitive dye (such as a ruthenium or platinum complex); the dye is selected for its photostability and specific quenching characteristics
Optical fiber or window: Carries excitation light from the source to the sensor tip and returns the emitted fluorescence to the detector; the use of optical fibers allows for non-invasive, remote sensing
Detection and electronics module: Contains the light source, photodiode or photomultiplier, and signal-processing electronics to determine phase or intensity changes
These components are often integrated into rugged industrial sensor design for use in process gas lines, environmental probes, or bioreactors, but the core measurement principle remains the same.
Benefits of quenched fluorescence
The adoption of quenched fluorescence systems in industrial measurement is driven by their optical simplicity and chemical robustness compared to traditional technologies. There are several benefits of quenched fluorescence:
Selectivity for oxygen: Quenched fluorescence is selective to oxygen, with negligible cross-sensitivity to water vapor, hydrogen sulfide, or carbon dioxide — species that often interfere with electrochemical sensors.
Part-per-million (ppm) concentrations
Long-term stability: Optical systems contain no consumable reagents or electrolytes. With stable dye matrices and solid-state components, calibration intervals are long and maintenance minimal.
Fast and continuous measurement: Because quenching is an instantaneous collisional process, fluorescence sensors respond in milliseconds to changes in oxygen concentration. This enables real-time monitoring of dynamic processes.
Safety and compatibility: Because these sensors operate optically and without sample contact with reactive elements, they can safely measure oxygen in hydrocarbon streams, flammable gases, or biological media without risk of ignition or contamination.
Quenched fluorescence compared to other oxygen measurement methods
Several other technologies are used for oxygen analysis, each with unique strengths and limitations. Comparing them provides context for when quenched fluorescence offers the greatest value.
Quenched fluorescence
Operating principle: Optical detection of collisional quenching of excited dye
Operating principle: Tunable diode laser at a specific wavelength where oxygen absorbs the light
Typical range: %
Strengths: Non-contact optical measurement; can be used for in-situ or extractive measurements
Limitations: May have interference with other background gases; dust and aerosols may coat over mirrors and windows
Compared to other oxygen measurement methods, quenched fluorescence offers a unique blend of speed, stability, and resilience in chemically aggressive or moisture-rich environments.
Calibration, performance, and innovation
Temperature and pressure compensation
The diffusion of oxygen through the sensor layer and the fluorescence lifetime of the dye are both temperature dependent. Therefore, most systems include automatic temperature compensation, often using a co-located thermistor. Pressure compensation may also be necessary for gas-phase measurements.
Sensor lifetime
Over years of operation, sensor films may experience gradual dye photobleaching or surface fouling. However, with modern materials, sensor lifetimes exceeding three to five years are common.
Calibration and maintenance
Calibration typically involves exposing the sensor to known oxygen concentrations (e.g., nitrogen for zero and air for span). Because of their stability, fluorescence-based sensors require infrequent recalibration compared to electrochemical alternatives.
Advanced materials
New sensor matrices — such as sol-gel hybrids, silica nanoparticles, and fluorinated polymers — are expanding the operating range and environmental tolerance of fluorescence-quenching sensors. These materials enhance dye stability and reduce photobleaching.
Multiplexed optical sensing
Recent advances in optical-fiber networks and miniaturized photonics are enabling multi-parameter sensors, combining oxygen, pH, and temperature measurement in a single probe.
Lifetime-based imaging
In biological and microfluidic research, fluorescence-lifetime imaging microscopy (FLIM) uses the same principles to produce spatial oxygen maps at microscopic scales, revealing gradients critical to cell behavior and metabolic processes.
Natural gas processing - Oxygen ingress into natural gas streams can cause corrosion, create explosive mixtures, and degrade product quality. Optical fluorescence sensors provide continuous, accurate oxygen measurement from gathering to distribution, helping operators maintain system integrity.
Energy transition – For carbon capture, utilization, and storage (CCUS) applications, oxygen is a contaminant that must be removed. Biogas/biomethane applications rely upon anaerobic fermentation so oxygen must be measured to determine if leaks in the digestor occur. Final biomethane quality must also have oxygen at low ppm levels. Green hydrogen applications have oxygen measurement requirements as well.
Bioprocessing & fermentation - In biotechnology, dissolved-oxygen control is vital for cell metabolism. Fluorescence sensors are widely used in fermenters to avoid the drift and sterilization issues of electrochemical probes.
Environmental & water monitoring - Fluorescence quenching measures dissolved oxygen (DO) in natural waters and wastewater. These sensors offer durability and low maintenance for long-term deployments.
Medical & Life Sciences - From tissue oxygenation to microfluidic systems, fluorescence sensors enable non-invasive, optical oxygen mapping in small volumes, essential for physiological and pharmacological studies.
Aerospace & energy applications - Immune to electromagnetic interference, fiber-based quenched fluorescence systems serve aerospace testing, combustion research, and fuel-cell monitoring, where precision and response speed matter.
Frequently asked questions about quenched fluorescence
Bi se radi udeležili našega dogodka? Izberite ustreznega glede na želeno kategorijo ali panogo.
Cenimo vašo zasebnost
Uporabljamo piškotke, da bi lahko izboljšali vašo izkušnjo med brskanjem, zbirali statistične podatke za izboljšanje delovanja spletnega mesta in zagotavljali prilagojene oglase ali vsebine.
Z izbiro "Sprejmi vse" se strinjate z našo uporabo piškotkov.
Za podrobnosti si oglejte naš Pravilnik o piškotkih .